DOUT#.SOURCEID
Description
DOUT#.SOURCEID sets the digital output source ID, for sources that require an ID.
Examples
Usage
DOUT#.SOURCEID can be used to select the compare channel when DOUT#.SOURCE = 4 (Compare).
Code
The following commands set the source of digital output 2 to compare channel 1, and digital output 3 to compare channel 2.
--> DOUT2.SOURCE 4
--> DOUT2.SOURCEID 1
--> DOUT3.SOURCE 4
--> DOUT3.SOURCEID 2
Context
For more information see Digital Inputs and Outputs.
Versions
Action | Version | Notes |
---|---|---|
Implemented | 02-00-00-000 | |
Added Compare channel support | 02-06-00-000 |
General Information
Type | Read/Write |
Units | N/A |
Range | 1 to 2 |
Default Value | 0 |
Data Type | Integer |
See Also | N/A |
Stored in Non-Volatile Memory |
Yes |
Variants Supported
All variants are supported
Fieldbus Information
Command |
Index |
SubIndex |
Data Type |
Units |
Float Scale |
Access |
PDO Mappable |
---|---|---|---|---|---|---|---|
DOUT1.SOURCEID |
360ah |
02h |
Unsigned8 |
- |
- |
Read/Write |
No |
DOUT2.SOURCEID |
360bh |
02h |
Unsigned8 |
- |
- |
Read/Write |
No |
DOUT3.SOURCEID |
360ch |
02h |
Unsigned8 |
- |
- |
Read/Write |
No |
DOUT4.SOURCEID |
360dh |
02h |
Unsigned8 |
- |
- |
Read/Write |
No |
DOUT5.SOURCEID |
360eh |
02h |
Unsigned8 |
- |
- |
Read/Write |
No |
DOUT6.SOURCEID |
360fh |
02h |
Unsigned8 |
- |
- |
Read/Write |
No |
DOUT7.SOURCEID |
3610h |
02h |
Unsigned8 |
- |
- |
Read/Write |
No |
DOUT8.SOURCEID |
3611h |
02h |
Unsigned8 |
- |
- |
Read/Write |
No |
DOUT9.SOURCEID |
3612h |
02h |
Unsigned8 |
- |
- |
Read/Write |
No |
ID |
Instance |
Attribute |
Name |
Data Type |
Access |
User Mappable |
---|---|---|---|---|---|---|
21200 |
1 |
21200 (0x52d0) |
DOUT1.SOURCEID |
Unsigned8 |
Read/Write |
Yes |
21201 |
1 |
21201 (0x52d1) |
DOUT2.SOURCEID |
Unsigned8 |
Read/Write |
Yes |
21202 |
1 |
21202 (0x52d2) |
DOUT3.SOURCEID |
Unsigned8 |
Read/Write |
Yes |
21203 |
1 |
21203 (0x52d3) |
DOUT4.SOURCEID |
Unsigned8 |
Read/Write |
Yes |
21204 |
1 |
21204 (0x52d4) |
DOUT5.SOURCEID |
Unsigned8 |
Read/Write |
Yes |
21205 |
1 |
21205 (0x52d5) |
DOUT6.SOURCEID |
Unsigned8 |
Read/Write |
Yes |
21206 |
1 |
21206 (0x52d6) |
DOUT7.SOURCEID |
Unsigned8 |
Read/Write |
Yes |
21207 |
1 |
21207 (0x52d7) |
DOUT8.SOURCEID |
Unsigned8 |
Read/Write |
Yes |
21208 |
1 |
21208 (0x52d8) |
DOUT9.SOURCEID |
Unsigned8 |
Read/Write |
Yes |
Parameter |
PNU |
Data Type |
Access |
Units |
---|---|---|---|---|
DOUT1.SOURCEID |
21200 |
Unsigned8 |
Read/Write |
- |
DOUT2.SOURCEID |
21201 |
Unsigned8 |
Read/Write |
- |
DOUT3.SOURCEID |
21202 |
Unsigned8 |
Read/Write |
- |
DOUT4.SOURCEID |
21203 |
Unsigned8 |
Read/Write |
- |
DOUT5.SOURCEID |
21204 |
Unsigned8 |
Read/Write |
- |
DOUT6.SOURCEID |
21205 |
Unsigned8 |
Read/Write |
- |
DOUT7.SOURCEID |
21206 |
Unsigned8 |
Read/Write |
- |
DOUT8.SOURCEID |
21207 |
Unsigned8 |
Read/Write |
- |
DOUT9.SOURCEID |
21208 |
Unsigned8 |
Read/Write |
- |